Part Number: TCA9555
Other Parts Discussed in Thread: TCA9535
Hello Expert,
My customer is using TCA 9555. I received the following question, Is it possible to cooperate in preparing answers? <Question> There are pins trying to use the IO pin of TCA9555 at the output.
CTA9555:
www.tij.co.jp/.../tca9555.pdf
This pin is connected to the input pin of DTC123JM of Rohm digital transformer. At the time of start-up (from power-on to setting completion), the voltage of this pin changes at 0.7 V, The DTC123JM is not turned on unintentionally. I want to turn off DTC 123JM at startup. I am trying to add a pull-down to this circuit, but please tell me the recommended pull-down resistance value.
DTC123JM
www.rohm.co.jp/.../DTC123JM
We are sorry for the inconvenience caused by the contents concerning
connection with other company's products.
Also, please tell the customer if there are points to check.
Best,Regars.
Nori