Part Number: DP83867E
I have a customer who is evaluating the DP83867E for their application and they have several questions regarding the operation:
We are evaluating the DP83867E for use in a future application (1000BT) which requires us to understand link drop/detect times.
Regarding link drop:
What value is T1 set to and which register is used to set this value? TI is shown in figure 19 on page 34, but no timing information is given for T1 in this diagram.
The datasheet states that in the T1 timer period there are several criteria allowed to generate link loss even and drop the link, including:
1. Loss of descrambler sync
2. Receive errors
3. MTL3 errors
4. Mean Squared Error (What does this mean? I do not see it defined in the 802.3 spec nor the PHY spec)
5. Energy Loss
What exactly would cause the link to drop? For example - would the link drop if only 1 receive error occurred in the T1 time period? If not – how many errors would need to be received during T1 for the link to drop?
Regarding link detection:
How long does it take to detect a link, assuming Auto-MIDX and Auto-Negitionation are both disabled? The data sheet mentions a Fast Link Detect feature (section 9.4.6.5), but it does not indicate what the standard link detects times are and what the fast link detect times are.
Thanks for your help with this.
Richard Elmquist