This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RE: BQ25890H: USB-PD support with Li-Ion charger?

Other Parts Discussed in Thread: TUSB321AI, BQ24600, BQ25606, TUSB422, BQ25890

Dear Jeff

Thank you very much for your answer.
After your post and more research I figured out, that USB-PD power supplies only do the handshake on the CC lines of the USB type C connector (pin A5 and B5).

So my mistake is, that I need a CC controller IC like the TUSB321AI. If  I am right, this IC should tell the charger to deliver 5V at 3A. After that, the charger IC gets the energy on the VBUS lines (A4, A9, B4, B9) without any handshakes on the USB data lines (A6, A7, B6, B7) required.

So if I am right, I can take a even simpler charger IC without any hand shaking like a standalone charger for example BQ25606 (3A max) or BQ24600 (10A max) in this case.


Question to the forum:
If I want to charge a big battery pack with 20Ah in our industry project. Can you recommend a good solution (easy to handle (no BGA), low complexity (no I2C) and lower price) for a CC controller and a standalone charger of TI? I thought about the TUSB422 to set the USB-PD supply to 20V and 3A (60W)  and then charge with the BQ24600 (10A max).
1) I saw that the TUSB422 required I2C and is available in BGA housing with 0.4mm pitch only. Especially the package is quite tricky for our processes. Isn't there a standalone version to force the USB-PD charger to 20V and 3A in a QFN housing?

2) I saw the BQ24600 is quite powerful and can handle up to 4 cells. Does TI has a simpler version for one cell (similar to BQ25606) but for higher currents (eg. 10A)?

Thank you for your comments!

Felix

  • Regarding the battery charger question, the QFN packaged, integrated FET bq25890 family charger can handle up to 5-A. For larger charge currents, we have the charge controller with external FETs, like the bq246xx family. The external FETs are required for heat dissipation. You might be able to use two bq2589x chargers in parallel as explained at www.ti.com/.../slyt651. Managing the power dissipation will still be a concern at 10-A.

    I have copied this post to the USB group form so that can answer the question about the USB IC.