Part Number: TPS65982
Other Parts Discussed in Thread: TPS65981
How would you pair the system with each other, so that we can supply the system either by the USB Type C or a plug.
We want to deliberately supply the system and not supply another system via USB-Type-C, so the starter kit is the sink.
Or is it not sensible to consider the system only as a sink?
I would still have some open points to the TPS65982:
- Is it possible to send data (in addition to the use of the TPS65982 also data) (keyword: USB3.0 - DRD)?
- Is your own firmware required? Not adjustable via bootstrapping?
O Can the firmware be imported via I2C?
- Is there a variant with -40..85 ° C (TPS65981)?
O What is the difference to the TPS65981?
- Is the TPS6598x detected when it is supplied (not the same as the Type-C as well as External)?
REGARDS,
Kamal