Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB925Q-Q1: selecting internal oscillator for OSC clock source

Guru 29720 points

Part Number: DS90UB925Q-Q1

Hi Team,

I believe internal oscillator is selected for OSC clock source when I set the following register regardless of external PCLK is supplied.

- 0x03[1] = 0 (Disable auto-switch)
- 0x14[2:1] = 01 (33 MHz Oscillator)

Is my understanding correct?

Best Regards,
Yaita / Japan disty