This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21520: CMTI

Genius 4870 points

Part Number: UCC21520

I found CMTI spec in datasheet following.

CMTI:Min 100V/ns

Does this mean min 100KV/us ?

Unit of CMTI of Other ISO part is KV/us.

regards,

  • Hello Kura,

    I am an application engineer with TI and will address your questions. The CMTI specification in the UCC21520 datasheet of 100V/ns is the same as the 100kV/us specification in some ISO devices. The us to ns conversion cancels the K in the KV units.

    Let me know if this answers your questions.

    Regards,

    Richard Herring