Part Number: TPS65982-EVM
Other Parts Discussed in Thread: TPS65982
I have bought 2x TPS65982-EVM and 1x Totalphase Aardvark to be able to do the following testing.
I am planning to test the different supported PD profiles from several USB type-C notebook power supplies.
So I would like to know how to configure/program the TPS65982-EVM to emulate every possible PD profile (20V/15V/14,5V/12V/9V/5V)
Below you will find the RX Source cap from one of the USB Type-C notebook power supplies.
Rx Source Cap (0x30)
Re-read Register Clear Status
Status: Register Read SUCCESS
numPDOs 6
PDO1: MaxCurrent or Power 3000 mA
PDO1: Min Voltage or Power 5000 mV
PDO1: Peak Current 0 PeakCurrentType_100PercentIOC
PDO1: Dual Role Data False
PDO1: USB Comm Capable 2
PDO1: Externally Powered True
PDO1: USB Suspend Supported False
PDO1: Dual Role Power False
PDO1: Supply Type Fixed
PDO2: MaxCurrent or Power 3000 mA
PDO2: Min Voltage or Power 9000 mV
PDO2: Max Voltage 0 PeakCurrentType_100PercentIOC
PDO2: Supply Type Fixed
PDO3: MaxCurrent or Power 3000 mA
PDO3: Min Voltage or Power 12000 mV
PDO3: Max Voltage 0 PeakCurrentType_100PercentIOC
PDO3: Supply Type Fixed
PDO4: MaxCurrent or Power 3000 mA
PDO4: Min Voltage or Power 15000 mV
PDO4: Max Voltage 0 PeakCurrentType_100PercentIOC
PDO4: Supply Type Fixed
PDO5: MaxCurrent or Power 2500 mA
PDO5: Min Voltage or Power 18000 mV
PDO5: Max Voltage 0 PeakCurrentType_100PercentIOC
PDO5: Supply Type Fixed
PDO6: MaxCurrent or Power 2200 mA
PDO6: Min Voltage or Power 20000 mV
PDO6: Max Voltage 0 PeakCurrentType_100PercentIOC
PDO6: Supply Type Fixed
So prefferably I am looking for a solution with only 1 Firmware that I need to program on the TPS65982-EVM and to be able to set the different PD profiles using switches or the onboard S1 dip switches. Can anyone help me to set this firmware accordingly? Thank you in advance