This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Rahul,
Thank you for your support.
do you confirm the base FW ver 1.12.05 support that automatic swap?
Thanks,
Andrew
Hi Andrew,
Yes, all of our official releases including 1.12.05 supports this feature.
Thanks,
Rahul
Dear Rahul:
I checked 1.12.06 FW released note, but I don't see bug fixed list showed AUX pin polarity swap automatic as assignment E.
Could you make sure it? Or it post on the other document?
Hi Rahul,
As I tested so far, the auto swapping of AUX on pin assignment E of UFP_D is not operating properly.
I set the UFP_D capability as pin assignment E only for the test purpose and built two FW that one with MUX SWAP BIT enabled and one with disabled as a default.
and the type-C mux was configured to receive pin assignment E.
I was only able to see a video when the MUX SWAP bit is enabled.
can you check again that the auto swapping is working on "UFP_D" side as well?
thanks,
Andrew
Rahul,
I don't think i can make test setup for DFP_D test. but i believe it works because initial Type-C to DP/HDMI gender was always working with DFP_D of PC.
do you have any status update for the UFP_D debugging?
Thanks,
Andrew