Part Number: TPS65983B
Other Parts Discussed in Thread: TPS65982,
We’re currently looking to use the TPS65982 in a new design. Could I please get help in answering the questions I have below?
Is there any concerns/caution in implementing a PP_EXT only source (i.e. to turn off the PP_5V0 and PP_HV) that would provide 5V to the VBUS? (Note: we would be implementing the TPS65982 as a source only + DFP along with the alpine ridge chip)
-
- Could we also just use one of the FETs for the PP_EXT? As we would only be sourcing 5V (3A)?
- Could the voltage sensing and current sensing also work for the 5V (3A) use case? I.e. to limit the current at 3A and set the over voltage protection to just over 5?
- Can this be configured via the TI configuration tool?
- The interest of using the external power to support the 5V and 3A is to reduce the max voltage drop that would occur within the TI chip (RDSon of up to 60mOhm would equate to up to 180mV of drop from 5V going to the USB C connector, based on the max 3A current) and also avoid excessive heat dissipation on the part.
- Would it be possible to route the PCH USB lines to the USB_RP on the TPS65982 (for the multiplexor function) instead of from the alpine ridge USB port?
Should we be using the TPS65983 of TPS65983B instead for Alpine Ridge?