This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83620: DP83620 RMII interface, Master Mode TX_CLK routing and reference clock

Part Number: DP83620


Dear All,

   I am experiencing some problem with the ethernet on a custom board and I am checking the connection between MAC and the PHY.  

   I am using DP83620 with RMII interface in master mode. The 25 MHz clock from the CPU crystal is provided to the X1 pin of the PHY, through a CLK_OUT pin of the CPU.

Now the RMII MAC requires the following signals - other than MDIO and MDC - (look for instance to SNLA076A for the DP83848 Table 1):

REF_CLK

TX_EN

TXD[0] 

TXD[1]

RXD[0]

RXD[1]

CRS_DV

Now, looking at the datasheet (par 6.2.1) it seems that for RMII (Master Mode) the signals CLK_OUT, RX_CLK and TX_CLK has to be routed to the MAC while for RMII (Slave Mode), the datasheet (par 6.2.2) says: "RX_CLK, TX_CLK, and CLK_OUT should not be used as the RMII reference clock in this mode but may be used for other system devices.": what does it means?

In my board (PHY configured in RMII Master Mode) the RX_CLK is routed to the REF_CLK of the MAC. Is this correct? I wonder if it is correct to say that RX_CLK and TX_CLK signal are synchronous with CLK_OUT.

Thank you.