Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB211-Q1: How to detect ENA_HS

Part Number: TUSB211-Q1
Other Parts Discussed in Thread: TUSB211

Hi,

Could you tell me how the TUSB211-Q1 detect HS mode in detail?

i.e.) detect voltage, timing, etc

The TUSB211 misdetects HS mode on the customer's system.

Best Regards,

Kuramochi 

  • Hello Kuramochi-san,

    The 211 checks DP and DM for pull-up or pull-down to determine if the link is High-Speed or not. High-speed devices will start by connecting as a full speed device (1.5k to 3.3V). Once it has been attached, it will do a high-speed chirp during reset and establish a high-speed connection if the hub supports it. If the device operates in high-speed mode, then the pull-up resistor is removed to balance the line.

    Regards,
    Diego.