Part Number: DP83867IR
Other Parts Discussed in Thread: DP83867ERGZ-R-EVM
Using DP83867IR with XE232-1000-FB374 processor. XE232 SGMII connections to RX_D0 and RX_D2 have weak pull downs. Resistance value not provided just maximum input source/sink current of (-/+)100uA.
Q1) Is it recommended to add additional pull down resistors at the DP83867IR?
Q2) If required, what is the recommended value, 2.49K?
The physical distance between the MAC and PHY is ~1" with trace matching per DATA Sheet.
Q3) Should matching external pull down resistors be added to RD_X1 and RX_D3 nets?
RJ45 connection: New to Ethernet, The Eval board and DS both show the "TD_[P:M]_C" pair connections are inverted as compared to the other three A, B & D pairs. This is for normal operation, straight cable connections, RJ45 connector pins 5 and 4, are per dot polarity of the transformer, reversed going into the transformer cable side and not corrected, inverted a second time, on the PHY side of the transformer.
Q4) Why?