This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1042-Q1: Floating Terminals

Guru 29720 points

Part Number: TCAN1042-Q1

Hi Team,

I believe TXD is pulled up to VCC when VIO is folating for TCAN1042DRQ1.
Is my understanding correct?



2)
I believe RXD doesn't have pull up feature like TXD above.
Is my understanding correct?

Best Regards,
Yaita / Japan disty

  • Hello Yaita-san,

    TXD is internally pulled to VCC in TCAN1042 and to VIO in TCAN1042V. If VIO is not powered, the device will be in an undervoltage lock-out state and keep the outputs high impedance.

    You are correct that there is not an internal pull-up on the RXD output.

    Regards,
    Max