Part Number: UCC5350
Hi all,
Do you have a plan like this?
Single isolated Gate Driver
With Miller clamp function
Propagation delay typ. 50ns
Thanks,
H.DOI
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: UCC5350
Hi all,
Do you have a plan like this?
Single isolated Gate Driver
With Miller clamp function
Propagation delay typ. 50ns
Thanks,
H.DOI
Hi Hiroshi,
I am an applications engineer for high power gate drivers.
The UCC5350MCD has a typical propagation delay of 65-ns and a maximum of 100-ns.
Which application are you using the isolated single channel gate driver that requires 50-ns typ. propagation delay?
We currently do not have plans for a new UCC5350MCD with lower prop. delay.
Regards,
Mateo
Mateo-san,
Thank you for your support for my customer.
I's 1kW DCAC for industrial mkt. 4pcs of SiCFET use. High-side x2 Lo-side x2.
Bus voltage is 800V so UCC2x52xx cannot meet Japanese PSE raw rule even if two pin rejected.
Primary to Secondary isolation distance is 7.6mm. so UCC53xx cannot meet.
ISO54xx is higher price than other maker.
Another maker have 8 pin but 8mm pri-sec. distance isolated gate driver.
And show the data of propagation delay matching for each other. This is point.
My customer very afraid of shoot-through.
Do you have good solution?
Thank you,
H.DOI
Mateo-san,
TI can make SOIC(DW) 10 package ?
If not , TI will lost many time.
I think that all Jap. maker evaluate SiC FET from now, use BM60015FV-LB
Tr, Tf are not so good. but it is acceptable.
Hiroshi-san,
Thank you for the valuable information.
Currently we do not have 10-pin isolated devices.
Regards,
Mateo