Part Number: SN65LVDM176
Hi
1.
Is there limitation of maximum output current from R terminal (1 pin) for the receiver?
2.
According to the Figure 11, 12 of datasheet, sink current is ~55mA and source current is ~62mA.
Are these maximum?
3.
As for R terminal (1 pin), does the output voltage depend on output current? (Output load?)
BestRegards