Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB928Q-Q1: Enable only I2S while disabling OLDI outputs

Part Number: DS90UB928Q-Q1

Hi Team,

Please advise me on questions bellow.

Q1, The register address 0x02 bit 7 control enable/disable OLDI outputs
(datasheet says CMOS output but may be OLDI)
When is bit is set to disable OLDI, is I2S outputs also disabled?

Q2. If so, are there any register bits which configure Enable I2S while Disable OLDI?

Q3.The datasheet insist as bellow. But it is not clear to me.
Is this bit set to ‘0’ (Disable output) in UN-LOCK state and needed to be set to ‘1’
In order to get outputs?

LVCMOS Output Enable. Self-clearing on loss of LOCK
0: Disable, Tristate Outputs (default)
1: Enable

Mita