Part Number: UCC20225
Hi,
A short question. How will ucc20225 react to a DC 5V input on PWM pin? I saw the signal rate of ISO72xx can be 0 Mbps. I want to know if ucc20225 is the same.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: UCC20225
Hi,
A short question. How will ucc20225 react to a DC 5V input on PWM pin? I saw the signal rate of ISO72xx can be 0 Mbps. I want to know if ucc20225 is the same.
Thanks.
Hello Jerry,
I am an applications engineer for the UCC20225.
OUTA will output a high signal while OUTB will output a low signal if 5Vdc is applied to the PWM input.
Please ensure that VCCI is greater than the 5V DC input for proper operation. Table 3 shows the logic operation of the UCC20225.
regards,
Mateo