Part Number: DP159RSBEVM
Other Parts Discussed in Thread: TMDS181
Two issues:
1.There are some mistakes in the user´s guide of the Evaluation Module DP159RSBEVM:
sllu224a
a) In the schematics page 4 is double and page 6 (with the reset button) is missing
b) In the description of the Eye Scan software (chapter 2.7 on page 8) you can read:
"Please note that Eye Scan cannot be performed when the device is in retimer mode, it does not function in redriver mode."
Which one of this modes work with Eye Scan?
2. Is it possible to use the HDMI input port for evluating the HDMI to HDMI mode instead of DisplayPort to HDMI? how to set the Jumpers and other things (Software?)?