This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b



Hi,

I am using LG G3 VS985 cell phone and it has installed android(version 4.4). Couple of days ago, I forcefully stop the app running on it. When I stop it, its OS gone crash giving error of Dload Memory. Two options were given that volume up for Dload Memory and volume down to reboot. If press volume up button then it gives the following error,"Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b".

And, if press the volume down button and reboot the device, then it displays the same error on screen. Sometime, it loaded the OS but as soon as after loading I try to open any app. It's crashed and gives the same error.

Please solve the issue.

Thanks,