Part Number: TPS65986
Hello,
We have a custom board using TPS65986 to control the input power. (UFP)
And we have two TPS65986 questions would need your help.
1. Does TPS65986 has GPIO event for Sink >5V
We saw TPS65986 has sink voltage event for 12V in application customization tool.
But in our case, we need GPIO event to control the system enable pin due to the input current limitation and system power consumption.
The system only can power up when the input voltage is more than 5V.
May I have your suggestion for this sink >5V event?
2.Could we update just one region by SPI interface?
As I know, there have two regions in the flash memory. And TPS65986 could update one region at one time by I2C interface.
And typically, we using I2C to update FW or using SPI for full flash.
But now our customer wants using SPI to update FW just for one region.
Could we update one region of flash at one time through SPI interface?
If we could do it, is there any document that we could reference?
Thanks