Part Number: HD3SS213
Hello,
Regarding to the V-by-one HS on HD3SS213, my customer is asking a question.
(Question)
Is this device supported V-by-one HS?
According to datasheet, the data rate of DA/B/C is up to 5.4 Gbps.
Therefore I think that it will be available to V-by-one HS. (4Gbps max)
If so, is there any point to notice or concern?
They will use 8 devices for 1:2 and 2:1 switch.
Regards,
Tao2199