Part Number: TCA9406
Team,
I have a customer who is asking for a layout example for the TCA9406. Since the part has an unusual pinout (SDA_A & SDA_B are on the same side), the Figure 8 Layout Example in the datasheet is wrong. This seems to have been brought up in another e2e thread as well:
About the Electrical Characteristics:
Min VOHA is specified as only "VCCA*0,67". This is not valid high-level. Usually VOH of a logic IC is 90% VCC. How can this IC be used for driving I2C input which expects minimum of 70% or 80% VCC? On the basis of the circuit description I would expect that the 10k resistors should pull output to VCCA-(10kR*20uA)=VCCA-0.2V. Could you please explain this?
The 10k resistors and One Shot Accelerators are missing in the datasheet specs. No min/max resistance/current values are given.
Thanks and Regards,
Mihir Gupta
FAE - South Germany