Part Number: SN65DSI84-Q1
Hi,
We are Vega Innovations Ltd and we are developing a high performance electric super car. Our prototype has been in development for the last three years and we plan to have a street drivable vehicle ready for testing and certification Q4 2017 with the ultimate goal of taking it into Production.
We are currently looking to expand into larger premises and have
Started on a 2nd prototype. There is huge potential in this project, our long-term plan is to produce mid-size vehicles, small city driving vehicles and provide conversions.
This is the link to our website. You can find detailed information there.
www.vega.lk
Our specialties also include,
High performance motor controllers
Efficient battery management system
Vehicle Control Unit
Charging Network Solution
Prototype testing
There is also a video on our Facebook page which details one of our launch tests.
https://www.facebook.com/VegaInnovations/videos/671219609715971/
While doing research on this, we came across your SN65DSI84-Q1. We're using SN65DSI84-Q1 with an NVIDIA TX2. Since the NVIDIA TX2 only has DSI outputs, we're using SN65DSI84-Q1 as the bridge.
Initialization Sequence Description
Init seq1 After power is applied and stable, all DSI Input lanes including DSI CLK(DA x P/N, DB x P/N) MUST be driven to
LP11 state.
Init seq2 Assert the EN pin
Init seq3 Wait for 1ms for the internal voltage regulator to stabilize
Init seq4 Initialize all CSR registers to their appropriate values based on the implementation (The SN65DSI84-Q1 is not
functional until the CSR registers are initialized)
Init seq5 Start the DSI video stream
Init seq6 Set the PLL_EN bit(CSR 0x0D.0)
Init seq7 Wait for a minimum of 3 ms.
Init seq8 Set the SOFT_RESET bit (CSR 0x09.0)
I uderstand seq 1,2 and 3. But appreciate if you can explain how seq 4,6 and 8 can be done. How do we program the SN65DSI84-Q1 registers?
Thank you.