This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ONET8501V: 10G-SR

Part Number: ONET8501V
Other Parts Discussed in Thread: ONET8551T, TIDA-00088

Hello,

I would like to develop a custom 10G BASE-SR module with 850nm ROSA/TOSA.

First we would like to evaluate different TOSA/ROSA modules ..

 

We have found the following documentation /EVM, which could be used in our test.

-TIDA-00088
-ONET-10G-EVM
-slla335.pdf

1, Which TI chipset you recommend as TIA and Laser driver ?

2, Can you provide us which EVM module could be used for initial test ?

3, Is the MSP430 software available for download ?

4, Does it support SFF-8472 compliant interface?

 

Many thanks,

 

Janos

 

 

  • Hi Janos,

    Thank you for your interest in our ONET devices. My understanding is that you are using a VCSEL-based TOSA for your application- is that correct?

    The TIDA-00088 and ONET-10G-EVM are reference design evaluation module/boards that are designed to demonstrate the performance of our DML laser driver ONET1151L, our 10G post-amplifier ONET1151P and our 10G TIA ONET8551T in an SFP+ LR module.

    So, in case you're using a VCSEL TOSA, we recommend you to take a look at our 10G VCSEL drivers ONET8501V and ONET1191V, along with our 10G post-amplifier ONET1151P and our 10G TIA ONET8551T.

    If you're interested to evaluate one or more of these devices, please send an email to onet1130ex_evm@list.ti.com.

    Hope this helps.

    Thanks,

    Sri