Part Number: MAX232
Dear all,
I would like to know the maximum distance that the MAX232IN can transmit/receive. Furthermore, I would like to know if the unconnected pins should i life free or grounded.
Many thanks
Cordially
Antonio
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MAX232
Dear all,
I would like to know the maximum distance that the MAX232IN can transmit/receive. Furthermore, I would like to know if the unconnected pins should i life free or grounded.
Many thanks
Cordially
Antonio
Antonio,
The distance of communication is governed by the load. In general the test of speicifc data rate is conducted with 3kOhm resistance and 1000pF capacitance. If low capacitanc cable is used, longer distance could still work. For example, UTP CAT-5 cable has a typical capacitance of 17 pF/ft, thus the maximum allowed cable length is about 58 feet.
For unused input pins, it's OK to ground them. For unused output pins, you can leave them open.
Regards,
Dear
Thank you so much for your help.
It is clear to me now. But, i need a bit of more help please.
Basically, I am connecting the 2 MAX232I between two Pics PIC16F1527-I/PT Master/Slave, Please could you help me to understand if i connect it well.
By the way i connected them in this way. (Slave PiC)The Tx Pin coming to the PIC to Pin 11 MAX232I T1IN, The Rx coming from the PIC to Pin 13 Max 232I R1IN.
Then: The PIn 14 MAX232I T1Out i connected to be my transmitter signal to be connected to the master pic and Pin 12 the receiver signal to be connected to the master PIC
Do you think is it right ?
Many thank
Antonio
Antonio,
Maybe I didn't fully understand the system setup. I think digital pins (TIN pin 11 and ROUT pin 12) should be connected to corresponding PIC port. Let TOUT pin 14 and RIN pin 13 to handle RS232 signaling.
Regards,