Part Number: TPS65982
I would like to implement the TPS65982 as a DRP. In this mode, I would like to support the charge through audio feature. The unit will be connected to a USB-C PD device operating in DFP mode. The audio jack will be configured as depicted in the USB PD Spec (appendix A). Can the presence of <Ra be sensed on CC1 and CC2 in this mode? Furthermore, can the register bit be exposed as a GPIO to actively switch between data and audio on DN DP?
A second mode will be required as well, negotiated from a DRP. In this mode, there will be the afformentioned USB-C PD DFP power source, but with the TPS65982 acting as a host to a USB type A port.
A third mode will be the same as above, with no USB-C PD device attached. In this mode, the TPS65982 will act as a data host and power source to a USB type A port
The final mode will be where the TPS65982 is acting as a power sink, and data client.
There will be a external processor available, but it would be best if it wasn't directly involved, particularly in the fourth mode. In the first mode, I imagine that there will need to be external processor involvement to react to the presence of Ra on the CC, and to generate a switch from data to audio. It would be a slam dunk if no involvement.