Part Number: DP83822IF
Other Parts Discussed in Thread: TLK105L
Hi team,
My customer is using DP83822 in their project with fiber port. However they met abnormal communication issue: After power up, communication is ok, if they plug out the fiber port and plug in again, then sometimes the communication will fail and the fail picture as showed in below picture:
Below are the registers value when normal communication and abnormal communication:
Normal situation registers:
MII PHY #1 transceiver registers(from 1st register to 32 register):
2100 784d 2000 a240 01e1 0000 0004 2001
0000 0000 4100 1000 0000 0000 0000 0000
0005 0108 e000 0000 0000 0000 0100 00e5
0400 8001 0000 007d 05ee 0000 0002 0000.
Basic mode control register 0x2100: Auto-negotiation disabled!
Speed fixed at 100 mbps, full-duplex.
Basic mode status register 0x784d ... 784d.
Link status: established.
Capable of 100baseTx-FD 100baseTx 10baseT-FD 10baseT.
Able to perform Auto-negotiation, negotiation not complete.
Vendor ID is 08:00:28:--:--:--, model 36 rev. 0.
No specific information is known about this transceiver type.
I'm advertising 01e1: 100baseTx-FD 100baseTx 10baseT-FD 10baseT
Advertising no additional info pages.
IEEE 802.3 CSMA/CD protocol.
Link partner capability is 0000:.
Negotiation did not complete.
#
For abnormal situation:
MII PHY #1 transceiver registers(from 1st register to 32 register)::
2100 784d 2000 a240 01e1 0000 0004 2001
0000 0000 4100 1000 0000 0000 0000 0000
2a05 0108 8300 0000 00ff ffff 0100 00e5
0400 8001 0000 007d 05ee 0000 0002 0000.
Basic mode control register 0x2100: Auto-negotiation disabled!
Speed fixed at 100 mbps, full-duplex.
Basic mode status register 0x784d ... 784d.
Link status: established.
Capable of 100baseTx-FD 100baseTx 10baseT-FD 10baseT.
Able to perform Auto-negotiation, negotiation not complete.
Vendor ID is 08:00:28:--:--:--, model 36 rev. 0.
No specific information is known about this transceiver type.
I'm advertising 01e1: 100baseTx-FD 100baseTx 10baseT-FD 10baseT
Advertising no additional info pages.
IEEE 802.3 CSMA/CD protocol.
Link partner capability is 0000:.
Negotiation did not complete.:
Below are the schematic that customer used:
Pls note that(Customer use our TLK105L before, so here they use same symbol of TLK105L for DP83822, so some pin name is a little bit confused). We also tried to remove the R1014 and R1015 away, the issue still the same.
As customer may go to MP stage, can you help look into this issue, thanks a lot for your great support on this issue!
Best regards,
Sulyn