Part Number: SN65HVD230
Hi team,
I'm using our SN65HVD230 to design a ADAS product. I'd like to use the Vref pin to stabilize the common mode voltage. Our product has strict limit on ESD ratings. We have to pass 15kV ESD test. I just wonder if i attach the Vref pin to the split termination resistor, will the ESD rating be degraded?
I can see from the datasheet that the rating for the CANH and CANL pin is 15kV but all other pins(including Vref pin) are 4kV.
Thanks.
Best regards.