This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO5452: Is 10ohm resister connected to VCC1 terminal mandatory?

Part Number: ISO5452

 Hello guys,

 One of my customers is going to evaluate ISO5452. They are designing PCB schematic for the evaluation and they have the following question at this moment.

Q. on Fig49/50/51 etc in ISO5452 datasheet (SLLSEQ4B), 10ohm resister is connected to VCC1. Is this resister mandatory for ISO5452 using? I think the resister is for noise filtering on VCC1 and it is not mandatory. Also I think it depends on VCC1 noise level.

 Could you please give me any answer or comment?

 Your answer would be much appreciated.

 Best regards,

 Kazuya Nakai.