Part Number: TS3USB221A
Dear team,
When using TS3USB221A with Vcc=3,3V is Vctrl=5V a valid condition? Looking at the ABSmax and shown test conditions in the datasheet with Vctrl=Vih it should. However, the recommended conditions refer the levels to VCC and it is not 100% clear if exceeding Vcc is valid.
thanks
Lutz