Part Number: HD3SS213
Hello,
Regarding to the power consumption on HD3SS213, my customer is asking some question.
(Question)
What is the power consumption at all port(DA0(n/p) to DA3(n/p)) switching?
According to datasheet(page 5), Supply current is 1mA(max).
(@VDD = 3.6 V,Dx_SEL or AUX_SEL = VDD or GND)
Based on the above data, we estimate that the total power consumption is not so large.
(There is the description "HD3SS213 <10mW" on the datasheet 1 page.)
From PCB layout example (page17) and EVM, it seems that the heat sink can be set.(Below)
Therefore they have a concern of whether there is possible that the total power consumption get large.
Regards,
Tao2199