Part Number: TPS65982-EVM
Hi All,
I have succesfully created several firmwares for different kind of PD profiles. However when I use the PD profile 14.5V which the Type-C power adapter should support I only get 5V as voltage output. I also noticed when reading the PD profile from the Power Adapter it does not show the PD 14.5V I read somewhere that the TPS65982-EVM does not support this profile. Is this correct? or is there a way to test the 14.5V PD profile?