Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS30EA101: Issues with Part - Looking for Pin and Footprint Compatible Part

Part Number: DS30EA101
Other Parts Discussed in Thread: LMH0394

Is there a pin and footprint compatible part to the DS30EA101 that is just a buffer and does not have equalization capabilities (or can be turned off)?

I am using this part in the system and the eye looks clean at the input, but the output glitches. Bypassing the equalizer results in correct operation, but we would like a component that adds additional margin (input sensitivity, etc.). The signal is from the DS30EA101 to a FPGA with input sensitivity of 100 mV.