Part Number: TPS65982-EVM
I can't seem to get the Aarvard tool to load. When I do a scan, I it cannot find the aardvark drivers. I have installed the aardvark drivers, but nowhere is there a aardvark.dll. What can I do?
Here is the error message:
Exception Encountered during I2C Test Read:Error importing aardvark.dll
Architecture of aardvark.dll may be wrong
No module named aardvark
DLL load failed: The specified module could not be found.
<type 'exceptions.ImportError'>
Details:
Traceback (most recent call last):
File "acConfigurationGui.py", line 1800, in test_read
File "hw_interface.pyc", line 128, in hw_open
ImportError: Error importing aardvark.dll
Architecture of aardvark.dll may be wrong
No module named aardvark
DLL load failed: The specified module could not be found.