Part Number: DP83848T
Other Parts Discussed in Thread: DP83620
Hi,
I have a question for the clock oscillator of the DP83848T. Indeed I need to change the oscillator.
For the clock we are using an oscillator at 25MHz with load capacity of 30pF.
I have to change the clock but I cannot understand something.
In the section 7.2.1.2.2 Crystal, it is written a 20pF load crystal resonator, while in the table 7.3 with the quartz specs it is written a Cload between 25 and 40pF.
On the market there are many available oscillator with Cload of 18pF. Can these oscillators at 18pF work well together with DP83848T?
Many Thanks,
Fax