Part Number: TCA9406
Other Parts Discussed in Thread: TMP102,
Hi
I am using this Device for Level Translation in I2C bus
The following is the schematic diagram attached
3.3V is connected to MC and few of the devices (TMP102) and a I/O expander ,ALS chip SI1133
and 1.8V is connector to few image sensor IC
when this out put pin is enabled and the I/O expander board not powered (disconnected ) we are facing some detection issue in an ALS chip
while debugging if we pull this line OE low their is still voltage available at both ends of the line
as per the datasheet if the Line is pulled Low their should not be any voltage on both ends It should be floating
but we are able to see some voltage always
how can we avoid this we have disconnected pull ups at all the lines but still issue is consistent