Part Number: TUSB320EVM
Other Parts Discussed in Thread: TUSB321, TUSB320
Hello,
I have two TUSB320EVMs that I would like to setup in the below method:
EVM #1 is a DFP set to advertise 3 Amps.
EVM #2 is a UFP in GPIO mode to allow the LEDs to show the current advertisement of the DFP.
Right now it is working so that the UFP in GPIO mode is correct and is showing the DFP is advertising default current mode (UFP Out1=High, Out2=Low).
Is there a way I can modify the EVM to have the DFP advertise 3 Amps? Other than to write it through I2C?
Thank you for the help!
Reed