Part Number: TCA6424A
Hi all
We would like to confirm the method which is sequencial read from Configuration Port0 to Configuration Port2 as the description on the datasheet P26.
Our customer would like to read the data from Configuration Port0 to Configuration Port2 sequencially(in a row).
In this case, as the description "if Input Port 1 is read, the next byte read is Input Port 0" on the datasheet, we have to set command byte = 0x0E(Port2), right? Or 0x8C?
(We are sorry that we could not understand Auto-increment function exactly. Is it used for data from Lower byte to Upper byte?)
If our recognition is not correct, could you let us know?
Kind regards,
Hirotaka Matsumoto