Part Number: SN65LVDS822
I am redesigning a circuit for compatibility with a display that has a clocking rate of 10MHz. This involves replacing a 75LVDS82 with a 65LVDS822 and a PCB re-spin.
I have 4 questions, which are,
1.Are both devices compatible with respect to the input differential and common-mode levels? My reading of the data-sheets suggest they are.
2.Do I need 100R differential matching resistors on the input of the 65LVDS822? (as was the case with the 75LVDS82).
3.In the 75LVDS82 based circuit 27R resistors were placed in series with each of the RGB output lines presumably for EMC. Are these required with the 65LVDS822 if I set the SLEW to '0' or open. The clocking speed is 10MHz
4.At the modest clock speed of 10MHz how critical are the RGB track lengths and impedance.