Part Number: TCA9534
It appears that a line is missing in table 6.3 "Recommended Operating Conditions" for Vin,H. As of today, it is only specified for Vcc = 1.65V to 2.7V. However, the Vin,L is specified for Vcc=1.65V to 2.7V and for Vcc = 3V to 5.5V. My application will use Vcc = 3.3V and the input signals to the P port will be 0V to 5.5V maximum. What is the Vinh specification for Vcc = 3V to 5.5V?