Part Number: LMH0394
When the LMH0394 is in the bypass mode (bypassing the equalizer), what is the "minimum input sensitivity" of the part? Specifically, if the frequency of the input matters, for a 200 MHz Nyquist signal input requirement when bypassing the EQ of the LMH0394. We would like to use this part as a buffer without taking advantage of the equalization capability.