Other Parts Discussed in Thread: SN65HVD3086E
Hi,
Can you help with below for a customer using the SN65HVD3086E ?
SN65HVD3086E current drain, MSOP10 package: If the unused transmitter is disabled (pin 4 [DI]=Vss and pin 3 [DE]=Vss) what resistors (fail safes or termination), if any, are required for the lowest supply current, Icc? For the same question of minimum supply current Icc, what pin connections are required for the receiver when disabled? pin 2 [/RE]= 5V pin 8[B] and pin 9[A] resistor connections to: Fail safes? Termination? Resistor values? Thanks