Part Number: TPS2551
Other Parts Discussed in Thread: TPS2553D
Hello,
I am planning to use TPS2551QDBVRQ1 in an application where I have to limit the USB current (Ioc) to 150mA. (USB/voltage should disable if someone draws more than 150mA). For achieving Ioc = 150mA, I need about 158K Ohms limiting resistor. But the datasheet recommends not to use more than 80Kohm. In that case, is it adviseable to use this chip for this application (with 160K)? What will be the imapct? Will I losse accuracy or life time or why it was recommended not to go above 80K . Please advise.
Thanks