This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVDS94: D0 Data Line signal Simulation

Part Number: SN65LVDS94

  1. When performing a simulation with 60Mbps data rate (D0 signal simulated with 30MHz signal in simulation) and a 10pF capacitor at data output, the signal looks almost triangle rather than a square wave as expected.
  2. When the load capacitor is connected through a transmission line the signal gets worse as the transmission line is longer (for instance -  2" transmission line) and an internal ripple is added (that gets noticed with a transmission line larger than 1")
  3. The clock output signal on the other hand looks good at 60MHz signal

 

Is this the case with actual device or is this only a model problem?