Part Number: DS15BA101
Other Parts Discussed in Thread: DS90UB933-Q1
Hi all,
As the title suggests, I would like to know whether it is possible to extend the STP cable length of the DS90UB93{3,4}-Q1 SerDes pair to 50+ meters by placing the DS15{B,E}A101 pair in between, as demonstrated in http://www.ti.com/lit/an/snla112e/snla112e.pdf.
The input to the DS90UB933-Q1 serializer is a 1080p30 image sensor, whose PIXCLK is adjustable.
This question arose as the application note provided above only mentioned FPD-Link II Embedded Clock signals. Further research revealed that FPD-Link III (that the DS90UB93{3,4}-Q1 pair operates on) is based on CML, which is also supported by the DS15{B,E}A101 extender pair.
We write this post to request some confirmation of our application.
Sincerely,
Adrian Yuen