Part Number: TUSB9261
Hi, everyone!
Recently, I have been working on a project with TUSB9261I which is used to interface with sata disk device and usb2.0. But now, we have a problem: my PC cannot recognize the sata disk after I power on my demo PCB , but I think the disk is running or doing sth when I touch the surface of the disk, I can feel it ( but the DC power source shows the current of my demo is only 0.2A) , also, my demo board can download the firmware which is provided on TI's website successfully ,and the Flash Burner can recognize the firmware version , by the way, I'll list some testing conditions below:
1. HS_FS_CONNECT#(PIN15) , PWR_STATE1(PIN14) , PWR_STATE0(PIN9) , SW_HB (PIN8) are permanently be low voltage;
2. HS_FS_SUSPEND#(PIN10) , SS_CONNECT#(PIN16) are permanently blinking or being high voltage when I try two different sata disk .
3. The models of my two exprimental disk are MHW2060BH( FUJITSU 5V@0.6A) and HTS543280L9SA00(HITACHI 5V@0.7A), and I have tried to connet them to my PC directly, PC can recognize them in
this situation.
4. The power and reset sequence is : 1V1 power comes first before 3V3 power , and then hold reset signal at low voltage for 2ms to release it .
5. There is a 40 MHz crystal that is clocking TUSB9261 - both FREQSEL0 and FREQSEL1 pins are pulled up using a 4k7 ohm resistors.
This pro is planned to use in one of our multiview products, please help me with this problem or give me some advice to solve it, thank you very much !
Best Regards,
Harson Zhang