Part Number: TUSB2046B
Hello,
For the PN: TUSB2046BIVFR the EOL notice states that the replacement PNs are: TUSB4041IPAPR or TUSB2046BVFR.
I have found that for the PN: TUSB2046BVFR the difference is the operating temperature rating. Is this true?
For the PN: TUSB4041IPAPR I have found that it is not a form or fit replacement, but has similar functionality.
My question has to do with an exact replacement for this PN, where it is a form/fit/function replacement with the same parameters, and have actually found a different PN: TUSB2046IBVFR, that was not specified in the EOL notice, and appears to be the exact equivalent to the EOL PN.
Is the PN: TUSB2046IBVFR the true exact equivalent to PN: TUSB2046BIVFR? If so, can an updated EOL notice be provided?
I appreciate your help. Thanks!
Regards,
Elizabeth Schneider