Part Number: TPS65982
If we’re going to use only the PP_EXT,
- Would I still need to connect the TI part’s VBUS to the EXT_VBUS?
- Do I leave the “5 to 20V” and “5V” inputs to the TI part as a “no connect” or do they have to be connected to GND?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS65982
If we’re going to use only the PP_EXT,