This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH0303: SDO output

Part Number: LMH0303

The datasheet states (page 13, register 0x04 named output) that >> 4:0 AMP 10000 SDO output amplitude in roughly 5 mV steps. <<

The default is 10000, which is 16 x 5 mV => 80mV! Is the datasheet correct or should it be in 50mV steps? Or an offset from 800mV?

Thanks