Part Number: HD3SS215
We are using the HD3SS215 in our system as a 1:2 switch. Typically, the DDC signal is 5V from an HDMI connector. Can the chip be setup to take in input 5.0V DDC signals and output DDC signals at 3.3V? Meaning pins J3 and J7 would see at 5V input signal, and pins H8, J8, H5, and J5 are all 3.3V output signals (with a 3.3V pull-up)?
My question would be can the blue-circled lines enter as 5V and the green-circled lines exit as 3.3V (if pulled up correctly)?
Thanks,
James